gpio配置

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

gpio配置

3,537 次查看
marry
Contributor I

mcu为ke06系列

  如何把大部分的pin配置为GPIO。

  现在我想把大部分的pin设置为gpio,该配置哪个寄存器,使其成为GPIO

标签 (1)
标记 (3)
0 项奖励
回复
11 回复数

3,187 次查看
ivadorazinova
NXP Employee
NXP Employee

Dear 文星 马,


I´m not sure what you exactly mean.

GPIO signal Descriptions is described in following table, page 678

gpio_2.png

If you mean GPIO/FGPIO register bits assignment, please go to Reference Manual for KE06, page 679

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MKE06P80M48SF0RM.pdf?fasp=1

gpio_a.png

gpio_b.png

I hope the information help you,

Best Regards,

Iva

0 项奖励
回复

3,187 次查看
Fan_xy
Contributor III

Hi Iva,

For example , how to configure the multiple pin "PTB1" to GPIO function .

Thank


0 项奖励
回复

3,187 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello fan xy,

please, try it by this way:

GPIOB_PDDR |= GPIO_PDDR_PDD(1<<1);  //PTB1 as output

GPIOB_PCOR |= GPIO_PCOR_PTCO(1<<1);  //set PTB1 to log0

You can  also invite drivers and examples (for gpio), which can help you.

Freescale Freedom Development Platform for Ki|Freescale

fsl.png

I hope it helps you,


Best Regards,

Iva


0 项奖励
回复

3,187 次查看
Fan_xy
Contributor III

Hi,

Thank  for your reply !

Maybe i did not say clearly.

I know this two instruction is to configure the gpio direction and data. While i want to know how to configure the pin to GPIO fuction.

For example "PTB1" pin, this pin can be used to "UART0_TX" "ADC0_SE5" or "GPIO" function,

and how to configure it to "GPIO" or "UARTO_TX" .

Thank

0 项奖励
回复

3,187 次查看
egoodii
Senior Contributor III

See my previous statement.  And find your processor's section on Pin Muxing in the manual, along with the Port Control register set.

0 项奖励
回复

3,187 次查看
Fan_xy
Contributor III

Hello Earl,

Thank you !

On the KE06 chip, there is no this register PORTB_PCR .

0 项奖励
回复

3,187 次查看
egoodii
Senior Contributor III

Well, now we're showing my general lack of familiarity with the KE06 in particular.  But downloading the manual MKE06P80M48SF0RM.pdf, section 10.2.1 details which 'alternate zero thru seven' will select for a pin, the first paragraph of which has this statement:

The Port Control Module is responsible for selecting which ALT functionality is available on each pin.

I assumed that was TRUE, and hence my prior suggestions.

That being said, I SEE YOUR POINT -- chapter 11, Port Control, makes NO mention of such Port Control Registers (as I use in the 'K' family).

It appears that for this family SOME control is REALLY in the SIM_PINSELx registers (12.2.4&5).  But I'm afraid I have to agree with you on this one!  It is NOT obvious how this works.  In the table on page 141, PTB1 can serve as PTB1, KB0_P9, UART0_TX, and ADC0_SE5 (default).  So I can see how UART0PS can move UART0 'away' from PortB (although i DON'T see how you keep UART0 from taking ANY I/O pins, maybe if it is not 'clock enabled'?), but that can't POSSIBLY be the whole story!

SO, I have to 'bow out' on being ANY HELP AT ALL (SORRY!), and we need to find someone more familiar with KE to help!

0 项奖励
回复

3,187 次查看
davidsherman
Senior Contributor I

The pins usually default to GPIO functionality.  In the example you give where you have UART and ADC pins shared with GPIO, turning on the UART transmit enable or receive enable bits then use the pins that are assigned for that purpose.  In the case of the ADC, turning on the ADC channel enable bits assign those pins to the ADC.  I'm not sure who wins if you have more than one function turned on, but having experienced the ADC taking control of a pin used for a SPI clock, all I can say is watch out for conflicts with pin functions.

0 项奖励
回复

3,187 次查看
egoodii
Senior Contributor III

Do NOT |= to PCOR.  Read always returns zero, so read-modify-write (to 'or in') is a waste of code&time.

But more to the apparent question, pin function is configured in the pin-mux control, so Port Control needs to select GPIO function, generally Alternative #1:

     PORTB_PCR1 = PORT_PCR_MUX(0x1);   //Select PTB1 as GPIO, might also add any OTHER configuration options for this pin!

0 项奖励
回复

3,187 次查看
ivadorazinova
NXP Employee
NXP Employee

You choose the function  on the pin. You cannot have more functions in the same time.

BR,

Iva

0 项奖励
回复

3,187 次查看
ivadorazinova
NXP Employee
NXP Employee

If you want to read data, you must read PDIR (Port Data Input Register).

Please, see p. 683

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MKE06P80M48SF0RM.pdf?fasp=1

BR,

Iva

0 项奖励
回复