TWR-KM34Z75M demo source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-KM34Z75M demo source

Jump to solution
1,954 Views
samdexter
Contributor II

TWR-KM34Z75M tower board comes with pre-installed demo program to test the buttons, LCD, etc.

Trying different things, particularly SDK examples, overwrites it and, so far, I didn't find a site

to download the demo source files...

If anybody knows where to get them, or by any chance has them, please share.

Thank you very much,

Sam.

0 Kudos
Reply
1 Solution
1,784 Views
shawn_shi
NXP Employee
NXP Employee

Hi Sam

please find attached FAT example.

Also the application use case could be helpful too.

BR

Shawn

View solution in original post

0 Kudos
Reply
2 Replies
1,785 Views
shawn_shi
NXP Employee
NXP Employee

Hi Sam

please find attached FAT example.

Also the application use case could be helpful too.

BR

Shawn

0 Kudos
Reply
1,784 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Sam Dexter,

How to: install KSDK 2.0  has illustrated the procedure of building KSDK, please refer to it for details.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply