TWR-KM34Z75M demo source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-KM34Z75M demo source

ソリューションへジャンプ
2,001件の閲覧回数
samdexter
Contributor II

TWR-KM34Z75M tower board comes with pre-installed demo program to test the buttons, LCD, etc.

Trying different things, particularly SDK examples, overwrites it and, so far, I didn't find a site

to download the demo source files...

If anybody knows where to get them, or by any chance has them, please share.

Thank you very much,

Sam.

0 件の賞賛
返信
1 解決策
1,831件の閲覧回数
shawn_shi
NXP Employee
NXP Employee

Hi Sam

please find attached FAT example.

Also the application use case could be helpful too.

BR

Shawn

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,832件の閲覧回数
shawn_shi
NXP Employee
NXP Employee

Hi Sam

please find attached FAT example.

Also the application use case could be helpful too.

BR

Shawn

0 件の賞賛
返信
1,831件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Sam Dexter,

How to: install KSDK 2.0  has illustrated the procedure of building KSDK, please refer to it for details.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信