SPI Baud Rate Clock Source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Baud Rate Clock Source

Jump to solution
4,235 Views
PeterFromSweden
Contributor III

I am confused by manual. In example a system frequency of 100 MHz is used. But implementing example gives only half the baud rate. I think the actual clock source is bus clock which is 50 MHz which would explain this. Can anyone confirm this?

K60 reference manual 3.4, Table 49-113.

/Peter

0 Kudos
Reply
1 Solution
3,417 Views
egoodii
Senior Contributor III

Absolutely!  The manual is misleading, presenting 100MHz data, given the 50MHz bus clock source.  DBR must be set to net a full 25MHz.

 

--ERGII

View solution in original post

0 Kudos
Reply
2 Replies
3,417 Views
egoodii
Senior Contributor III
0 Kudos
Reply
3,418 Views
egoodii
Senior Contributor III

Absolutely!  The manual is misleading, presenting 100MHz data, given the 50MHz bus clock source.  DBR must be set to net a full 25MHz.

 

--ERGII

0 Kudos
Reply