SPI Baud Rate Clock Source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Baud Rate Clock Source

ソリューションへジャンプ
4,392件の閲覧回数
PeterFromSweden
Contributor III

I am confused by manual. In example a system frequency of 100 MHz is used. But implementing example gives only half the baud rate. I think the actual clock source is bus clock which is 50 MHz which would explain this. Can anyone confirm this?

K60 reference manual 3.4, Table 49-113.

/Peter

0 件の賞賛
返信
1 解決策
3,574件の閲覧回数
egoodii
Senior Contributor III

Absolutely!  The manual is misleading, presenting 100MHz data, given the 50MHz bus clock source.  DBR must be set to net a full 25MHz.

 

--ERGII

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,574件の閲覧回数
egoodii
Senior Contributor III
0 件の賞賛
返信
3,574件の閲覧回数
egoodii
Senior Contributor III

Absolutely!  The manual is misleading, presenting 100MHz data, given the 50MHz bus clock source.  DBR must be set to net a full 25MHz.

 

--ERGII

0 件の賞賛
返信