SPI Baud Rate Clock Source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPI Baud Rate Clock Source

跳至解决方案
4,385 次查看
PeterFromSweden
Contributor III

I am confused by manual. In example a system frequency of 100 MHz is used. But implementing example gives only half the baud rate. I think the actual clock source is bus clock which is 50 MHz which would explain this. Can anyone confirm this?

K60 reference manual 3.4, Table 49-113.

/Peter

0 项奖励
回复
1 解答
3,567 次查看
egoodii
Senior Contributor III

Absolutely!  The manual is misleading, presenting 100MHz data, given the 50MHz bus clock source.  DBR must be set to net a full 25MHz.

 

--ERGII

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,567 次查看
egoodii
Senior Contributor III
0 项奖励
回复
3,567 次查看
egoodii
Senior Contributor III

Absolutely!  The manual is misleading, presenting 100MHz data, given the 50MHz bus clock source.  DBR must be set to net a full 25MHz.

 

--ERGII

0 项奖励
回复