PWMA/eFlexPWM Vs FlexTimer Module in KV4x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PWMA/eFlexPWM Vs FlexTimer Module in KV4x

跳至解决方案
2,676 次查看
Vishesh45
Contributor II

In KV4x Reference Manual there are two options to generate PWM

Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)

Chapter 39 : FlexTimer Module (FTM)

what is the difference between these two..??

with both i can successfully  able to generate complimentary pwm signals with deadtime insertion for my full bridge power supply application.

I aslo need to read CADC.

found the document for " FlexTimer and ADC Synchronization for Field Oriented Control on Kinetis ".

is it possible to use ADC in sync with PWM(Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)) .....same as FlexTimer..?

0 项奖励
回复
1 解答
2,585 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

I see that you have another case with the same question, I will follow up on this last one that I mention.

在原帖中查看解决方案

1 回复
2,585 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

I see that you have another case with the same question, I will follow up on this last one that I mention.