PWMA/eFlexPWM Vs FlexTimer Module in KV4x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWMA/eFlexPWM Vs FlexTimer Module in KV4x

ソリューションへジャンプ
2,676件の閲覧回数
Vishesh45
Contributor II

In KV4x Reference Manual there are two options to generate PWM

Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)

Chapter 39 : FlexTimer Module (FTM)

what is the difference between these two..??

with both i can successfully  able to generate complimentary pwm signals with deadtime insertion for my full bridge power supply application.

I aslo need to read CADC.

found the document for " FlexTimer and ADC Synchronization for Field Oriented Control on Kinetis ".

is it possible to use ADC in sync with PWM(Chapter 37 : Pulse Width Modulator A (PWMA/eFlexPWM)) .....same as FlexTimer..?

0 件の賞賛
返信
1 解決策
2,585件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

I see that you have another case with the same question, I will follow up on this last one that I mention.

元の投稿で解決策を見る

1 返信
2,585件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

I see that you have another case with the same question, I will follow up on this last one that I mention.