MKL25Z: VrefH input current?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKL25Z: VrefH input current?

ソリューションへジャンプ
2,078件の閲覧回数
frankvanhooft
Contributor III

Hello,

What's the input current drawn by the VREFH pin on the MKL25Z128 processor?  I can find total current draw of the ADC, but cannot find the input current of the reference pin in the datasheet. We're using a shunt reference, so this is an important number.

Thanks a lot.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,778件の閲覧回数
apanecatl
Senior Contributor II

The power consumption of the VrefH input ha snot been characterized apart from the whole ADC module however the figure is taken into consideration to obtain the ADC module power consumption.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,778件の閲覧回数
apanecatl
Senior Contributor II

The power consumption of the VrefH input ha snot been characterized apart from the whole ADC module however the figure is taken into consideration to obtain the ADC module power consumption.

0 件の賞賛
返信