MKL25Z: VrefH input current?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL25Z: VrefH input current?

Jump to solution
2,078 Views
frankvanhooft
Contributor III

Hello,

What's the input current drawn by the VREFH pin on the MKL25Z128 processor?  I can find total current draw of the ADC, but cannot find the input current of the reference pin in the datasheet. We're using a shunt reference, so this is an important number.

Thanks a lot.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,778 Views
apanecatl
Senior Contributor II

The power consumption of the VrefH input ha snot been characterized apart from the whole ADC module however the figure is taken into consideration to obtain the ADC module power consumption.

View solution in original post

0 Kudos
Reply
1 Reply
1,778 Views
apanecatl
Senior Contributor II

The power consumption of the VrefH input ha snot been characterized apart from the whole ADC module however the figure is taken into consideration to obtain the ADC module power consumption.

0 Kudos
Reply