MK20DX256VMC7 IDD_VBAT when VDD = 0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK20DX256VMC7 IDD_VBAT when VDD = 0

1,259 次查看
phil74
NXP Employee
NXP Employee

Hello,

Can you confirm that the RTC of MK20DX256  can still run on Vbat voltage even if main MCU Vdd = 0 , and then IDD_VBAT average current is Max 0.94µA at 3.0V, –40 to 25°C, according to datasheet?

Thanks in advance,

Best Regards,

Philippe

标签 (1)
0 项奖励
回复
1 回复

1,173 次查看
egoodii
Senior Contributor III

Yes, that operational understanding is correct.

0 项奖励
回复