Flashing MKW30Z over SWD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing MKW30Z over SWD

Jump to solution
1,876 Views
ivandrobyshevs1
Contributor II

I need to program MKW30Z via SWD, using another ARM chip's GPIO. It would be really helpful to see an example sequence for loading firmware to the chip, similar to the below code on github for EFM32. Is there  something like that in SDK, or may be in some open source project(s)?

PySWD/EFM32.py at master · disk91/PySWD · GitHub 

Thanks!

0 Kudos
Reply
1 Solution
1,730 Views
ivandrobyshevs1
Contributor II

Turned out that recent OpenOCD supports KW30Z, and I was able to program it that way.

View solution in original post

0 Kudos
Reply
1 Reply
1,731 Views
ivandrobyshevs1
Contributor II

Turned out that recent OpenOCD supports KW30Z, and I was able to program it that way.

0 Kudos
Reply