MK20DX256VMC7 IDD_VBAT when VDD = 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK20DX256VMC7 IDD_VBAT when VDD = 0

1,245 Views
phil74
NXP Employee
NXP Employee

Hello,

Can you confirm that the RTC of MK20DX256  can still run on Vbat voltage even if main MCU Vdd = 0 , and then IDD_VBAT average current is Max 0.94µA at 3.0V, –40 to 25°C, according to datasheet?

Thanks in advance,

Best Regards,

Philippe

Labels (1)
0 Kudos
Reply
1 Reply

1,159 Views
egoodii
Senior Contributor III

Yes, that operational understanding is correct.

0 Kudos
Reply