MK20DX256VMC7 IDD_VBAT when VDD = 0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK20DX256VMC7 IDD_VBAT when VDD = 0

1,243件の閲覧回数
phil74
NXP Employee
NXP Employee

Hello,

Can you confirm that the RTC of MK20DX256  can still run on Vbat voltage even if main MCU Vdd = 0 , and then IDD_VBAT average current is Max 0.94µA at 3.0V, –40 to 25°C, according to datasheet?

Thanks in advance,

Best Regards,

Philippe

ラベル(1)
0 件の賞賛
返信
1 返信

1,157件の閲覧回数
egoodii
Senior Contributor III

Yes, that operational understanding is correct.

0 件の賞賛
返信