K61 Mask Set Revision and JTAG ID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K61 Mask Set Revision and JTAG ID

ソリューションへジャンプ
2,383件の閲覧回数
stevenmartin
Contributor I
  1. Is there anyway to read the mask set revision of a K61 device via SW and/or JTAG?
  2. Table 61-2 of the K61 reference manual lists the fields of the JTAG ID register. The PRN and PIN fields are listed as 0 and TBD respectively. What are the current values of these fields? Do they ever get updated? 
ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
2,252件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Answer to your questions, please see below:

1. There no way to read the maskset directly, however by reading the device revision numbers (REVID), we provide corresponding maskset by below Engineering Bulleting EB782:

https://www.nxp.com/docs/en/engineering-bulletin/EB782.pdf

2. The part revision number (PRN), which is a copy of the SIM_SDID[REVID], may change for a mask revision, the EB782 had list it clearly.

The part identification number (PIN) is vary depending on the Kinetis family identification SIM_SDID[FAMID] and pin count identifications SIM_SDID[PINID] fields. This had been listed in the K61 RM as below:

pastedImage_1.png

元の投稿で解決策を見る

1 返信
2,253件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Answer to your questions, please see below:

1. There no way to read the maskset directly, however by reading the device revision numbers (REVID), we provide corresponding maskset by below Engineering Bulleting EB782:

https://www.nxp.com/docs/en/engineering-bulletin/EB782.pdf

2. The part revision number (PRN), which is a copy of the SIM_SDID[REVID], may change for a mask revision, the EB782 had list it clearly.

The part identification number (PIN) is vary depending on the Kinetis family identification SIM_SDID[FAMID] and pin count identifications SIM_SDID[PINID] fields. This had been listed in the K61 RM as below:

pastedImage_1.png