K61 Mask Set Revision and JTAG ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K61 Mask Set Revision and JTAG ID

Jump to solution
2,406 Views
stevenmartin
Contributor I
  1. Is there anyway to read the mask set revision of a K61 device via SW and/or JTAG?
  2. Table 61-2 of the K61 reference manual lists the fields of the JTAG ID register. The PRN and PIN fields are listed as 0 and TBD respectively. What are the current values of these fields? Do they ever get updated? 
Tags (2)
0 Kudos
Reply
1 Solution
2,275 Views
miduo
NXP Employee
NXP Employee

Hello,

Answer to your questions, please see below:

1. There no way to read the maskset directly, however by reading the device revision numbers (REVID), we provide corresponding maskset by below Engineering Bulleting EB782:

https://www.nxp.com/docs/en/engineering-bulletin/EB782.pdf

2. The part revision number (PRN), which is a copy of the SIM_SDID[REVID], may change for a mask revision, the EB782 had list it clearly.

The part identification number (PIN) is vary depending on the Kinetis family identification SIM_SDID[FAMID] and pin count identifications SIM_SDID[PINID] fields. This had been listed in the K61 RM as below:

pastedImage_1.png

View solution in original post

1 Reply
2,276 Views
miduo
NXP Employee
NXP Employee

Hello,

Answer to your questions, please see below:

1. There no way to read the maskset directly, however by reading the device revision numbers (REVID), we provide corresponding maskset by below Engineering Bulleting EB782:

https://www.nxp.com/docs/en/engineering-bulletin/EB782.pdf

2. The part revision number (PRN), which is a copy of the SIM_SDID[REVID], may change for a mask revision, the EB782 had list it clearly.

The part identification number (PIN) is vary depending on the Kinetis family identification SIM_SDID[FAMID] and pin count identifications SIM_SDID[PINID] fields. This had been listed in the K61 RM as below:

pastedImage_1.png