K61 Controller Ethernet Link Establish Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K61 Controller Ethernet Link Establish Problem

跳至解决方案
2,506 次查看
mani8421
Contributor II

 

We are working with KSZ8041NL for our requirement with K61 Controller.

 

when we are connecting the Ethernet cable to the Jack the two status LED’s simultaneously go ON and OFF continuously as long it is connected. And the link is not established between Host PC.


Can any suggest what could be the problem

标记 (3)
0 项奖励
回复
1 解答
2,367 次查看
hectorsanchez
Contributor IV

Hi Mani,

Looks like you have activity on the port and probably the jacks or the cable is not working as intended, try to change the cable and test the jack on another device.

Hope this helps,

Hector Sanchez

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,368 次查看
hectorsanchez
Contributor IV

Hi Mani,

Looks like you have activity on the port and probably the jacks or the cable is not working as intended, try to change the cable and test the jack on another device.

Hope this helps,

Hector Sanchez

0 项奖励
回复
2,367 次查看
mani8421
Contributor II

Hi Hector,

Thanks for the reply

     Problem is solved by changing the Ethernet Jack....

Thanks and regards,

      MANI

0 项奖励
回复