K61 Controller Ethernet Link Establish Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K61 Controller Ethernet Link Establish Problem

Jump to solution
2,477 Views
mani8421
Contributor II

 

We are working with KSZ8041NL for our requirement with K61 Controller.

 

when we are connecting the Ethernet cable to the Jack the two status LED’s simultaneously go ON and OFF continuously as long it is connected. And the link is not established between Host PC.


Can any suggest what could be the problem

Tags (3)
0 Kudos
Reply
1 Solution
2,338 Views
hectorsanchez
Contributor IV

Hi Mani,

Looks like you have activity on the port and probably the jacks or the cable is not working as intended, try to change the cable and test the jack on another device.

Hope this helps,

Hector Sanchez

View solution in original post

0 Kudos
Reply
2 Replies
2,339 Views
hectorsanchez
Contributor IV

Hi Mani,

Looks like you have activity on the port and probably the jacks or the cable is not working as intended, try to change the cable and test the jack on another device.

Hope this helps,

Hector Sanchez

0 Kudos
Reply
2,338 Views
mani8421
Contributor II

Hi Hector,

Thanks for the reply

     Problem is solved by changing the Ethernet Jack....

Thanks and regards,

      MANI

0 Kudos
Reply