K61 Controller Ethernet Link Establish Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K61 Controller Ethernet Link Establish Problem

ソリューションへジャンプ
2,476件の閲覧回数
mani8421
Contributor II

 

We are working with KSZ8041NL for our requirement with K61 Controller.

 

when we are connecting the Ethernet cable to the Jack the two status LED’s simultaneously go ON and OFF continuously as long it is connected. And the link is not established between Host PC.


Can any suggest what could be the problem

タグ(3)
0 件の賞賛
返信
1 解決策
2,337件の閲覧回数
hectorsanchez
Contributor IV

Hi Mani,

Looks like you have activity on the port and probably the jacks or the cable is not working as intended, try to change the cable and test the jack on another device.

Hope this helps,

Hector Sanchez

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,338件の閲覧回数
hectorsanchez
Contributor IV

Hi Mani,

Looks like you have activity on the port and probably the jacks or the cable is not working as intended, try to change the cable and test the jack on another device.

Hope this helps,

Hector Sanchez

0 件の賞賛
返信
2,337件の閲覧回数
mani8421
Contributor II

Hi Hector,

Thanks for the reply

     Problem is solved by changing the Ethernet Jack....

Thanks and regards,

      MANI

0 件の賞賛
返信