K53 : Power-Up Sequence about 5v tolerant GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K53 : Power-Up Sequence about 5v tolerant GPIO

Jump to solution
2,045 Views
koichisakagami
Contributor II

Dear community,
I have a question about power-up sequence for 5v tolerant GPIO .

Device is Kinetis K50.

[Question]
When VDD power is not turned on ,
Is it possible to add a 5v input voltage to the 5v tolerant GPIO ?

Best Regards,
Koichi Sakagami

0 Kudos
Reply
1 Solution
1,834 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

5 volt tolerant digital I/O pins are internally clamped to VSS through a ESD protection diode. There is no diode to VDD.

There is no problem to apply 5V input voltage on those pins when VDD without power up.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,835 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

5 volt tolerant digital I/O pins are internally clamped to VSS through a ESD protection diode. There is no diode to VDD.

There is no problem to apply 5V input voltage on those pins when VDD without power up.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,834 Views
koichisakagami
Contributor II

Dear Ma Hui san,

Thank you for your reply.

I got it .

Best Regards,

Koichi Sakagami

0 Kudos
Reply