Core lockup reset when erase a flash sector in KE02

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Core lockup reset when erase a flash sector in KE02

1,814件の閲覧回数
raysss
Contributor I

When I try to erase a flash sector in MKE02Z64VLD4,the core lockup reset is occured(the LOCKUP bit in SIM->SRSID is set).

the FTMRH registers config as:

FTMRH->FCLKDIV = 0x0f;//15.6~16.6MHz
FTMRH->FCNFG = 0x00;
FTMRH->FERCNFG = 0x00;

and the following functions for erasing a flash sector:

bool FlashPreCheck(void)

{

  if((FTMRH->FCLKDIV & FTMRH_FCLKDIV_FDIV_MASK) != 0x0f){

  if((FTMRH->FCLKDIV & FTMRH_FCLKDIV_FDIVLCK_MASK) != 0){

  NVIC_SystemReset();

  }

  else{

  if((FTMRH->FSTAT & FTMRH_FSTAT_CCIF_MASK) != 0){

  FTMRH->FCLKDIV = 0x0f;

  }

  }

  return FALSE;

  }

  if((FTMRH->FSTAT & FTMRH_FSTAT_CCIF_MASK) == 0){

  return FALSE;

  }

  if((FTMRH->FSTAT & FTMRH_FSTAT_ACCERR_MASK) != 0){

  FTMRH->FSTAT |= FTMRH_FSTAT_ACCERR_MASK;

  }

  if((FTMRH->FSTAT & FTMRH_FSTAT_FPVIOL_MASK) != 0){

  FTMRH->FSTAT |= FTMRH_FSTAT_FPVIOL_MASK;

  }

  __disable_irq();

  WDOG->CNT = 0x02A6;

  WDOG->CNT = 0x80B4;

  __enable_irq();

  return TRUE;

}

bool FlashEraseSector(u32 addr)

{

  u32 saddr;

  if(!FlashPreCheck())return FALSE;

  saddr = addr;

  __disable_irq();

  FTMRH->FCCOBIX = 0;

  FTMRH->FCCOBHI = 0x0a;

  FTMRH->FCCOBLO = (u8)(saddr >> 16);

  FTMRH->FCCOBIX = 1;

  FTMRH->FCCOBHI = (u8)(saddr >> 8);

  FTMRH->FCCOBLO = (u8)(saddr >> 0);

  FTMRH->FSTAT |= FTMRH_FSTAT_CCIF_MASK;

  while((FTMRH->FSTAT & FTMRH_FSTAT_CCIF_MASK) == 0);

  __enable_irq();

  if((FTMRH->FSTAT & FTMRH_FSTAT_MGSTAT_MASK) != 0)return FALSE;

  return TRUE;

}

Is anyone can help me?

ラベル(1)
0 件の賞賛
返信
1 返信

1,281件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Lei yue,

I'd like to suggest that you could refer to the Flash demo from the sample code of the FRDMKE02Z board at first.

In the Flash demo, there're a lot of flash operation functions, so please refer to it for details and download the sample code through the link as below.

If you have any other questions, please feel free to contact with me.

The link of the sample code:

cache.freescale.com/files/32bit/software/KE02-SC.zip
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信