K53 Internal Vref configuration and usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K53 Internal Vref configuration and usage

跳至解决方案
2,287 次查看
GeoD
Contributor I

I need to use the internal Vref to perform a single ended battery measurement.

On this proc selecting Valt for the ADC reference selects VrefOut.

No matter how VrefOut is configured the ADC always reads 0.

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,979 次查看
adriansc
Contributor IV

Hi,

If you are using a custom board would be helpful to check the SPF-26994_C , which you can download from here:

http://cache.freescale.com/files/microcontrollers/hardware_tools/printed_circuit_boards/TWR-K53N512-...

The schematic shows the way of how Vref are connected, there are some filters that recommend to use.

In the table below you can see the ADC operating conditions for K50 (This information is in K50 Reference Manual):

adc k50.png

Hope this helps.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,980 次查看
adriansc
Contributor IV

Hi,

If you are using a custom board would be helpful to check the SPF-26994_C , which you can download from here:

http://cache.freescale.com/files/microcontrollers/hardware_tools/printed_circuit_boards/TWR-K53N512-...

The schematic shows the way of how Vref are connected, there are some filters that recommend to use.

In the table below you can see the ADC operating conditions for K50 (This information is in K50 Reference Manual):

adc k50.png

Hope this helps.

0 项奖励
回复