K53 Internal Vref configuration and usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K53 Internal Vref configuration and usage

Jump to solution
2,377 Views
GeoD
Contributor I

I need to use the internal Vref to perform a single ended battery measurement.

On this proc selecting Valt for the ADC reference selects VrefOut.

No matter how VrefOut is configured the ADC always reads 0.

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
2,069 Views
adriansc
Contributor IV

Hi,

If you are using a custom board would be helpful to check the SPF-26994_C , which you can download from here:

http://cache.freescale.com/files/microcontrollers/hardware_tools/printed_circuit_boards/TWR-K53N512-...

The schematic shows the way of how Vref are connected, there are some filters that recommend to use.

In the table below you can see the ADC operating conditions for K50 (This information is in K50 Reference Manual):

adc k50.png

Hope this helps.

View solution in original post

0 Kudos
Reply
1 Reply
2,070 Views
adriansc
Contributor IV

Hi,

If you are using a custom board would be helpful to check the SPF-26994_C , which you can download from here:

http://cache.freescale.com/files/microcontrollers/hardware_tools/printed_circuit_boards/TWR-K53N512-...

The schematic shows the way of how Vref are connected, there are some filters that recommend to use.

In the table below you can see the ADC operating conditions for K50 (This information is in K50 Reference Manual):

adc k50.png

Hope this helps.

0 Kudos
Reply