K53 Internal Vref configuration and usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K53 Internal Vref configuration and usage

ソリューションへジャンプ
2,280件の閲覧回数
GeoD
Contributor I

I need to use the internal Vref to perform a single ended battery measurement.

On this proc selecting Valt for the ADC reference selects VrefOut.

No matter how VrefOut is configured the ADC always reads 0.

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,972件の閲覧回数
adriansc
Contributor IV

Hi,

If you are using a custom board would be helpful to check the SPF-26994_C , which you can download from here:

http://cache.freescale.com/files/microcontrollers/hardware_tools/printed_circuit_boards/TWR-K53N512-...

The schematic shows the way of how Vref are connected, there are some filters that recommend to use.

In the table below you can see the ADC operating conditions for K50 (This information is in K50 Reference Manual):

adc k50.png

Hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,973件の閲覧回数
adriansc
Contributor IV

Hi,

If you are using a custom board would be helpful to check the SPF-26994_C , which you can download from here:

http://cache.freescale.com/files/microcontrollers/hardware_tools/printed_circuit_boards/TWR-K53N512-...

The schematic shows the way of how Vref are connected, there are some filters that recommend to use.

In the table below you can see the ADC operating conditions for K50 (This information is in K50 Reference Manual):

adc k50.png

Hope this helps.

0 件の賞賛
返信