K21 secure storage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,367件の閲覧回数
PHXFAE
Contributor II

I have a customer who is using the K21 with the tamper protection.

They are at the point of wanting to use the K21 32 bytes of secure storage.

The data sheet says the minimum Vbat is 1.71V.  Is this the minimum to preserve the data in the 32 bytes?

What is the Vbat voltage to guarantee the 32 bytes of secure storage is cleared?

With the K21 unpowered except Vbat can a tamper event clear the 32 bytes?

Is the only way to clear the 32 bytes of secure storage to lower Vbat?

Thx for the help.

1 解決策
3,245件の閲覧回数
PatriciaTeran
Contributor III

Hi, Alex

The VBAT min that you are refering to is the MIN for the RTC battery supply voltage (1.71V), if you go to section 2.2.1 of the datasheet, you will see the MIN voltage to retain the VBAT register file is between 0.8V - 1.5V, any less will be considered as a VBAT power-on reset  and it will erase the 32 byte VBAT register file.

The only way to clear the 32 bytes is during VBAT power-on reset, this module is not affected by the other reset types.

Hope it helps,
Regards!

Patricia Teran

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
3,246件の閲覧回数
PHXFAE
Contributor II

I am logged in and there is no button like you show anywhere on the page.

0 件の賞賛
返信
3,245件の閲覧回数
PHXFAE
Contributor II

Where is the correct answer button.  I don't see it.

0 件の賞賛
返信
3,246件の閲覧回数
PatriciaTeran
Contributor III

You have to Log in, in order to see it. It should be right below the post with the answer, like this 

   pastedImage_3.png

0 件の賞賛
返信
3,246件の閲覧回数
PatriciaTeran
Contributor III

Hi, Alex

The VBAT min that you are refering to is the MIN for the RTC battery supply voltage (1.71V), if you go to section 2.2.1 of the datasheet, you will see the MIN voltage to retain the VBAT register file is between 0.8V - 1.5V, any less will be considered as a VBAT power-on reset  and it will erase the 32 byte VBAT register file.

The only way to clear the 32 bytes is during VBAT power-on reset, this module is not affected by the other reset types.

Hope it helps,
Regards!

Patricia Teran

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------