K21 secure storage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K21 secure storage

跳至解决方案
3,473 次查看
PHXFAE
Contributor II

I have a customer who is using the K21 with the tamper protection.

They are at the point of wanting to use the K21 32 bytes of secure storage.

The data sheet says the minimum Vbat is 1.71V.  Is this the minimum to preserve the data in the 32 bytes?

What is the Vbat voltage to guarantee the 32 bytes of secure storage is cleared?

With the K21 unpowered except Vbat can a tamper event clear the 32 bytes?

Is the only way to clear the 32 bytes of secure storage to lower Vbat?

Thx for the help.

1 解答
3,351 次查看
PatriciaTeran
Contributor III

Hi, Alex

The VBAT min that you are refering to is the MIN for the RTC battery supply voltage (1.71V), if you go to section 2.2.1 of the datasheet, you will see the MIN voltage to retain the VBAT register file is between 0.8V - 1.5V, any less will be considered as a VBAT power-on reset  and it will erase the 32 byte VBAT register file.

The only way to clear the 32 bytes is during VBAT power-on reset, this module is not affected by the other reset types.

Hope it helps,
Regards!

Patricia Teran

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
3,352 次查看
PHXFAE
Contributor II

I am logged in and there is no button like you show anywhere on the page.

0 项奖励
回复
3,351 次查看
PHXFAE
Contributor II

Where is the correct answer button.  I don't see it.

0 项奖励
回复
3,352 次查看
PatriciaTeran
Contributor III

You have to Log in, in order to see it. It should be right below the post with the answer, like this 

   pastedImage_3.png

0 项奖励
回复
3,351 次查看
PatriciaTeran
Contributor III

Hi, Alex

The VBAT min that you are refering to is the MIN for the RTC battery supply voltage (1.71V), if you go to section 2.2.1 of the datasheet, you will see the MIN voltage to retain the VBAT register file is between 0.8V - 1.5V, any less will be considered as a VBAT power-on reset  and it will erase the 32 byte VBAT register file.

The only way to clear the 32 bytes is during VBAT power-on reset, this module is not affected by the other reset types.

Hope it helps,
Regards!

Patricia Teran

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------