I can't understand the mean of MKL15 package.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I can't understand the mean of MKL15 package.

跳至解决方案
1,520 次查看
wangbaode
Contributor IV

hello eyeryone,

I'm using MKL15Z128.but I can't understand the mean of MKL15 package.

pastedImage_0.png

in the picture from MKL15Z128 package document,eyery side has two numbers. Why?why has two numbers every side?

which number should be used in my package?

标记 (3)
0 项奖励
回复
1 解答
1,385 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Baode

As you know, every pin of chip has a plating layer on real metal. The dimension of outside line is plating dimension. The internal dimension of inside line is metal dimension.

Hope my reply can help you.

Best Regards

Paul

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,385 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi wang baode,

   Every side has two numbers, this two number are the size range,  it is the mechanical tolerance.

   When you draw your chip package, if your pin pitch is less 0.4, you should keep your width below 0.2, otherwise, the pin each to other maybe connected. But if your pin pitch is bigger than 0.4, you can draw your pin width a little

bigger than 0.2, for a food contact with silicon.

   About the length, you can draw it bigger than 0.23, for soldering.

  

pastedImage_0.png

I wish it helps you!

Best regards!

Jingjing

1,385 次查看
wangbaode
Contributor IV

oh,I see.Thank you.

0 项奖励
回复
1,386 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Baode

As you know, every pin of chip has a plating layer on real metal. The dimension of outside line is plating dimension. The internal dimension of inside line is metal dimension.

Hope my reply can help you.

Best Regards

Paul

0 项奖励
回复
1,385 次查看
Paul_Tian
NXP Employee
NXP Employee

The two dimensions on each side is mechanical tolerance.