I can't understand the mean of MKL15 package.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I can't understand the mean of MKL15 package.

ソリューションへジャンプ
1,495件の閲覧回数
wangbaode
Contributor IV

hello eyeryone,

I'm using MKL15Z128.but I can't understand the mean of MKL15 package.

pastedImage_0.png

in the picture from MKL15Z128 package document,eyery side has two numbers. Why?why has two numbers every side?

which number should be used in my package?

タグ(3)
0 件の賞賛
返信
1 解決策
1,360件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Baode

As you know, every pin of chip has a plating layer on real metal. The dimension of outside line is plating dimension. The internal dimension of inside line is metal dimension.

Hope my reply can help you.

Best Regards

Paul

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,360件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi wang baode,

   Every side has two numbers, this two number are the size range,  it is the mechanical tolerance.

   When you draw your chip package, if your pin pitch is less 0.4, you should keep your width below 0.2, otherwise, the pin each to other maybe connected. But if your pin pitch is bigger than 0.4, you can draw your pin width a little

bigger than 0.2, for a food contact with silicon.

   About the length, you can draw it bigger than 0.23, for soldering.

  

pastedImage_0.png

I wish it helps you!

Best regards!

Jingjing

1,360件の閲覧回数
wangbaode
Contributor IV

oh,I see.Thank you.

0 件の賞賛
返信
1,361件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Baode

As you know, every pin of chip has a plating layer on real metal. The dimension of outside line is plating dimension. The internal dimension of inside line is metal dimension.

Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信
1,360件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

The two dimensions on each side is mechanical tolerance.