How can I add TWR-K70120M to the "Kinetics Studio"?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can I add TWR-K70120M to the "Kinetics Studio"?

跳至解决方案
2,457 次查看
omkardixit
Contributor III

Hi

How can I add TWR-K70120M to the Kinetics Studio?. Currently, I have only the following options.

Regards,

Omkar Dixit

Kinetis Design Studio.PNG

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,451 次查看
nxf58904
NXP Employee
NXP Employee

Hi,

In Processors ,it include K70.

I hope this can help you.

nxf58904_0-1609922741837.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

在原帖中查看解决方案

2 回复数
2,452 次查看
nxf58904
NXP Employee
NXP Employee

Hi,

In Processors ,it include K70.

I hope this can help you.

nxf58904_0-1609922741837.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

2,447 次查看
omkardixit
Contributor III

Hi

Thank you so much @nxf58904.

Regards

Omkar Dixit

0 项奖励
回复