How can I add TWR-K70120M to the "Kinetics Studio"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I add TWR-K70120M to the "Kinetics Studio"?

Jump to solution
2,506 Views
omkardixit
Contributor III

Hi

How can I add TWR-K70120M to the Kinetics Studio?. Currently, I have only the following options.

Regards,

Omkar Dixit

Kinetis Design Studio.PNG

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,500 Views
nxf58904
NXP Employee
NXP Employee

Hi,

In Processors ,it include K70.

I hope this can help you.

nxf58904_0-1609922741837.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

2 Replies
2,501 Views
nxf58904
NXP Employee
NXP Employee

Hi,

In Processors ,it include K70.

I hope this can help you.

nxf58904_0-1609922741837.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

2,496 Views
omkardixit
Contributor III

Hi

Thank you so much @nxf58904.

Regards

Omkar Dixit

0 Kudos
Reply