Help check the MK66FN2M0VLQ18 connect 16bit SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help check the MK66FN2M0VLQ18 connect 16bit SDRAM

2,789 次查看
hansonhe
NXP Employee
NXP Employee

Help check the MK66FN2M0VLQ18 connect 16bit SDRAM, use SDRAM type is IS42S16800F16bit data width.

标签 (1)
0 项奖励
回复
2 回复数

2,507 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Please referring to the reference design.

How to access SDRAM based on K65 SDRAM controller
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,507 次查看
hansonhe
NXP Employee
NXP Employee

Jeremy,

It is some different from K65 which use 32bit data width. Do you have 16bit data width design guide?

0 项奖励
回复