Help check the MK66FN2M0VLQ18 connect 16bit SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help check the MK66FN2M0VLQ18 connect 16bit SDRAM

3,876件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Help check the MK66FN2M0VLQ18 connect 16bit SDRAM, use SDRAM type is IS42S16800F,16bit data width.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,594件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Please referring to the reference design.

How to access SDRAM based on K65 SDRAM controller
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,594件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Jeremy,

It is some different from K65 which use 32bit data width. Do you have 16bit data width design guide?

0 件の賞賛
返信