Help check the MK66FN2M0VLQ18 connect 16bit SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help check the MK66FN2M0VLQ18 connect 16bit SDRAM

3,904 Views
hansonhe
NXP Employee
NXP Employee

Help check the MK66FN2M0VLQ18 connect 16bit SDRAM, use SDRAM type is IS42S16800F,16bit data width.

Labels (1)
0 Kudos
Reply
2 Replies

3,622 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Please referring to the reference design.

How to access SDRAM based on K65 SDRAM controller
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,622 Views
hansonhe
NXP Employee
NXP Employee

Jeremy,

It is some different from K65 which use 32bit data width. Do you have 16bit data width design guide?

0 Kudos
Reply