Freedom current capacity

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Freedom current capacity

2,015 次查看
georgealbertagu
Contributor I

What is the maximum current that can run through a Freedom board without the board burning?

0 项奖励
回复
3 回复数

1,829 次查看
apanecatl
Senior Contributor II

Do you refer to the board itself as if an electrical current were to magically circulate through the board; to the maximum current provided by a specific pin in a component? your questions is too general, you need to re formulate your question and be more specific.

0 项奖励
回复

1,829 次查看
georgealbertagu
Contributor I

Regarding power supply input. I have a 12V source that I am planning on converting down to 5V, but I do not know the current supplied so I want to be sure I will not burn my board

0 项奖励
回复

1,829 次查看
apanecatl
Senior Contributor II

The voltage regulator in the FRDM boards is NCP1117ST33T3G, its maximum rated output current is 1000mA; you can use that figure as a milestone.

0 项奖励
回复