Freedom current capacity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freedom current capacity

2,111件の閲覧回数
georgealbertagu
Contributor I

What is the maximum current that can run through a Freedom board without the board burning?

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,925件の閲覧回数
apanecatl
Senior Contributor II

Do you refer to the board itself as if an electrical current were to magically circulate through the board; to the maximum current provided by a specific pin in a component? your questions is too general, you need to re formulate your question and be more specific.

0 件の賞賛
返信

1,925件の閲覧回数
georgealbertagu
Contributor I

Regarding power supply input. I have a 12V source that I am planning on converting down to 5V, but I do not know the current supplied so I want to be sure I will not burn my board

0 件の賞賛
返信

1,925件の閲覧回数
apanecatl
Senior Contributor II

The voltage regulator in the FRDM boards is NCP1117ST33T3G, its maximum rated output current is 1000mA; you can use that figure as a milestone.

0 件の賞賛
返信