For the KL03 in QFN pkg., should the center pad be grounded?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For the KL03 in QFN pkg., should the center pad be grounded?

ソリューションへジャンプ
2,111件の閲覧回数
brenconsult
Contributor II

The datasheet doesn't appear to address the question of how to handle the exposed center pad of the QFN packages for the KL03 MCUs.  Ground it?  Leave it floating?

Thanks,

Scott

ラベル(1)
タグ(1)
1 解決策
1,970件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Scott,

I think that the Application Note AN1902​ is what you are looking for. It has relevant information regarding hardware considerations for the QFN packages. Please take a look specially in the section 4.2.2 Thermal/Electrical Pad Guidelines.

Best regards,

Earl Ramírez.

/* If this post answers your question please click the Correct Answer button. */

元の投稿で解決策を見る

3 返答(返信)
1,970件の閲覧回数
Stano
NXP Employee
NXP Employee

Hi Scott,

yes the exposed center pad has to be grounded.

Best Regards,

Stano.

1,970件の閲覧回数
brenconsult
Contributor II

Thank you!  Is this documented some place, and I just missed it?

Scott

0 件の賞賛
返信
1,971件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Scott,

I think that the Application Note AN1902​ is what you are looking for. It has relevant information regarding hardware considerations for the QFN packages. Please take a look specially in the section 4.2.2 Thermal/Electrical Pad Guidelines.

Best regards,

Earl Ramírez.

/* If this post answers your question please click the Correct Answer button. */