For the KL03 in QFN pkg., should the center pad be grounded?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For the KL03 in QFN pkg., should the center pad be grounded?

Jump to solution
1,060 Views
brenconsult
Contributor II

The datasheet doesn't appear to address the question of how to handle the exposed center pad of the QFN packages for the KL03 MCUs.  Ground it?  Leave it floating?

Thanks,

Scott

Labels (1)
Tags (1)
1 Solution
919 Views
EarlOrlando
Senior Contributor II

Hello Scott,

I think that the Application Note AN1902​ is what you are looking for. It has relevant information regarding hardware considerations for the QFN packages. Please take a look specially in the section 4.2.2 Thermal/Electrical Pad Guidelines.

Best regards,

Earl Ramírez.

/* If this post answers your question please click the Correct Answer button. */

View solution in original post

3 Replies
919 Views
Stano
NXP Employee
NXP Employee

Hi Scott,

yes the exposed center pad has to be grounded.

Best Regards,

Stano.

919 Views
brenconsult
Contributor II

Thank you!  Is this documented some place, and I just missed it?

Scott

0 Kudos
920 Views
EarlOrlando
Senior Contributor II

Hello Scott,

I think that the Application Note AN1902​ is what you are looking for. It has relevant information regarding hardware considerations for the QFN packages. Please take a look specially in the section 4.2.2 Thermal/Electrical Pad Guidelines.

Best regards,

Earl Ramírez.

/* If this post answers your question please click the Correct Answer button. */