Debug external MKV10Z16VLC7 target with FRDM-KV11Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug external MKV10Z16VLC7 target with FRDM-KV11Z

ソリューションへジャンプ
2,516件の閲覧回数
vijayvaidya
Contributor I

Hello,

1. Can FRDM-KV11Z board be used to debug MKV10Z16VLC7 based external target board.

2. What steps we need to follow. We are not able to conclude this from the information given in User Guide of FRDM-        KV11Z.

3. Any pointers for this will be most appreciated,

Thanks in advance,

Vijay Vaidya

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,415件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hello, Vijay

Here is a nice tutorial from MCU on eclipse that may help you. The KL43 is used as debugger

but the process must work on other FRDM boards.

https://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/

You will need to modify certain pins related to SDA interface on the board, details are contained in the tutorial.

 

On the other hand, have you checked out the LPC Link 2 debugger and programmer?

https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpc-li...

 

 I recommend you for the long term this handfull external debugger. 


Have a great day,
Diego

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,416件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hello, Vijay

Here is a nice tutorial from MCU on eclipse that may help you. The KL43 is used as debugger

but the process must work on other FRDM boards.

https://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/

You will need to modify certain pins related to SDA interface on the board, details are contained in the tutorial.

 

On the other hand, have you checked out the LPC Link 2 debugger and programmer?

https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpc-li...

 

 I recommend you for the long term this handfull external debugger. 


Have a great day,
Diego

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,415件の閲覧回数
vijayvaidya
Contributor I

Hello Diego,

Thanks a lot for your suggestions,

Best Regards,

Vijay Vaidya

0 件の賞賛
返信