DTM configuration for KW36

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DTM configuration for KW36

1,749 Views
nsuresh2
Contributor III

Hi estephania_martinez‌,

I configured KW36 DTM as mentioned in the below link (Through a 2-wire UART interface)

Direct Test Mode (DTM) Configurations for the KW family 

But to verify the DTM behavior I tested using the below commands

1. LE Reset 

    (a)  0x0000

    (b)  0x0204

    (c)  0x0300

2. LE Transmitter Test

      0x8000

3. LE Receiver Test

      0x4000

4. LE Test End

      0xC000

In the above-mentioned commands, LE Reset is not getting passed with all the 3 commands and LE Test End command is also failed.

Can you please check this issue?

Hardware used: USB to TTL converter (3.3v logic level)

Thanks!

Regards,

Naven Suresh

Tags (2)
0 Kudos
Reply
2 Replies

1,615 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Are you using test tool? Could you please share with me the complete command you sent and the response ?

Regards,

Estephania

0 Kudos
Reply

1,615 Views
nsuresh2
Contributor III

Hi,

Thanks for the response.

It is not the test tool. It is a third-party tool and now it is working fine the issue was in address configuration.

Thanks!

Regards,

Naven Suresh

0 Kudos
Reply