Configure Multiple ADC Channel and read conversion value using sw trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure Multiple ADC Channel and read conversion value using sw trigger

1,461 Views
shivangi_23
Contributor I

Hello, 

I am using MKM35z512vlq7 microcontroller . I need to configure 3 adc chanel  one for pot,2 temp sensor and 3 for current sense by using sw trigger . I need to read 3rd and 2nd channel in continuous mode .Can you tell me the approach how can i do this so that my all adc work properly and can not conflit with each other.

need your support as soon as possible.

0 Kudos
Reply
1 Reply

1,426 Views
vicentegomez
NXP TechSupport
NXP TechSupport

The KM35 only has 1 ADC module, so all the channels need to have the same clock configuration, because of this one option is that you read  2 channels on continuous mode and then reconfigure the ADC to read using trigger mode. the problem is that if you need good accuracy on the ADC measurements you will need to calibrate every time that you reconfigure the ADC, I do not know if this is an option for you

regards

0 Kudos
Reply