Kinetis / Latch input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis / Latch input

2,146 Views
asapuntz
Contributor I

Looking at KE1xF (or S32K14x)

PORTx->PCR[IRQC] allows an input pin to latch edges or levels which can then be read in PORTx->PCR[ISF] PORTx->ISFR. This is very handy to avoid missing transitions while software is busy with other activities.

However, it seems that this will produce in an interrupt (or DMA) if any pin on PORTx is configured to do so.

I've seen other (Cortex-M4) processors where masking of such interrupts is configurable on a per-pin (rather than per-port) basis. Is this level of control not available?

0 Kudos
Reply
3 Replies

2,101 Views
asapuntz
Contributor I

would be useful to have PORTx->PCR[IRQC] options which don't produce interrupts or DMA

0 Kudos
Reply

2,094 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

We will consider it for new MCU designs, thank you.

0 Kudos
Reply

2,102 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @asapuntz , sorry, but no, it is not available

0 Kudos
Reply