Configure Multiple ADC Channel and read conversion value using sw trigger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configure Multiple ADC Channel and read conversion value using sw trigger

1,569件の閲覧回数
shivangi_23
Contributor I

Hello, 

I am using MKM35z512vlq7 microcontroller . I need to configure 3 adc chanel  one for pot,2 temp sensor and 3 for current sense by using sw trigger . I need to read 3rd and 2nd channel in continuous mode .Can you tell me the approach how can i do this so that my all adc work properly and can not conflit with each other.

need your support as soon as possible.

0 件の賞賛
返信
1 返信

1,534件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

The KM35 only has 1 ADC module, so all the channels need to have the same clock configuration, because of this one option is that you read  2 channels on continuous mode and then reconfigure the ADC to read using trigger mode. the problem is that if you need good accuracy on the ADC measurements you will need to calibrate every time that you reconfigure the ADC, I do not know if this is an option for you

regards

0 件の賞賛
返信