Can't create MCUXpresso Project using MKM34Z256VLL7 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't create MCUXpresso Project using MKM34Z256VLL7 ?

Jump to solution
2,108 Views
GanesanGuru
Contributor IV

Hi team,

I've followed this link, for working with Custom HWs, where the SDK for LPCXpresso845MAX in imported and used to create a new breakout board.During the process, the device package has been modified/changed to suit the application. It worked perfectly for me without any glitches.

Similarly, I imported both SDK_2_14_0_TWR-KM34Z75M & SDK_2_14_0_MKM34Z256xxx7  -- and when i changed the default device package to MKM34Z256VLL7 (where my custom board is gonna be build based on this package), the project build without any error. But, when I go for the config tools- pin modifications in project I'm getting the below error.

Then to create a project for MKM34Z256VLL7? 

 

Screenshot from 2023-10-19 19-06-28.png

Labels (1)
0 Kudos
Reply
1 Solution
2,081 Views
GanesanGuru
Contributor IV

The issues has been rectified, once we enable the config tools with older MCU package and then switching to our necessary package (MKM34Z256VLL7).

View solution in original post

1 Reply
2,082 Views
GanesanGuru
Contributor IV

The issues has been rectified, once we enable the config tools with older MCU package and then switching to our necessary package (MKM34Z256VLL7).