Can't create MCUXpresso Project using MKM34Z256VLL7 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't create MCUXpresso Project using MKM34Z256VLL7 ?

ソリューションへジャンプ
2,104件の閲覧回数
GanesanGuru
Contributor IV

Hi team,

I've followed this link, for working with Custom HWs, where the SDK for LPCXpresso845MAX in imported and used to create a new breakout board.During the process, the device package has been modified/changed to suit the application. It worked perfectly for me without any glitches.

Similarly, I imported both SDK_2_14_0_TWR-KM34Z75M & SDK_2_14_0_MKM34Z256xxx7  -- and when i changed the default device package to MKM34Z256VLL7 (where my custom board is gonna be build based on this package), the project build without any error. But, when I go for the config tools- pin modifications in project I'm getting the below error.

Then to create a project for MKM34Z256VLL7? 

 

Screenshot from 2023-10-19 19-06-28.png

ラベル(1)
0 件の賞賛
返信
1 解決策
2,077件の閲覧回数
GanesanGuru
Contributor IV

The issues has been rectified, once we enable the config tools with older MCU package and then switching to our necessary package (MKM34Z256VLL7).

元の投稿で解決策を見る

1 返信
2,078件の閲覧回数
GanesanGuru
Contributor IV

The issues has been rectified, once we enable the config tools with older MCU package and then switching to our necessary package (MKM34Z256VLL7).