BOOTCFG pin active high or low

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BOOTCFG pin active high or low

ソリューションへジャンプ
2,408件の閲覧回数
wilco_work
Contributor I

Hello all,

I'm using the K82FN256 and want to use the BOOTCFG0 pin for booting. Is this BOOTCFG0 active HIGH or active LOW (asserted by logic 1 or 0)?

Kin regards

ラベル(2)
タグ(2)
1 解決策
2,292件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Jan,

Based on the following table of the reference manual. 

pastedImage_1.png

We can know that the pin is active high, asserted by logic 1. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,293件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Jan,

Based on the following table of the reference manual. 

pastedImage_1.png

We can know that the pin is active high, asserted by logic 1. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信
2,292件の閲覧回数
wilco_work
Contributor I

Hi Victor,

Thank you! Apparently putting a high value at the pin will result in a 1 at the register. I missed that point.

Kind regards