BOOTCFG pin active high or low

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BOOTCFG pin active high or low

跳至解决方案
2,386 次查看
wilco_work
Contributor I

Hello all,

I'm using the K82FN256 and want to use the BOOTCFG0 pin for booting. Is this BOOTCFG0 active HIGH or active LOW (asserted by logic 1 or 0)?

Kin regards

标记 (2)
1 解答
2,270 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Jan,

Based on the following table of the reference manual. 

pastedImage_1.png

We can know that the pin is active high, asserted by logic 1. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,271 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Jan,

Based on the following table of the reference manual. 

pastedImage_1.png

We can know that the pin is active high, asserted by logic 1. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 项奖励
回复
2,270 次查看
wilco_work
Contributor I

Hi Victor,

Thank you! Apparently putting a high value at the pin will result in a 1 at the register. I missed that point.

Kind regards