48 MHz clock generation using external reference in KL17

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

48 MHz clock generation using external reference in KL17

跳至解决方案
2,533 次查看
felicita
Fresh Out Contributor

Hi all,

We have designed our custom board with MKL17Z256VFM4, with 16 MHz external reference crystal.

Is it possible to generate 48 MHz using external reference clock?

Thank you!

Regards,

Felicita Mercy D.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,416 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Felicita Mercy,

     No, you can't use the external 16Mhz crystal get 48Mhz core clock.

    Please refer to the KL17 reference manual:

pastedImage_1.png

    You can find the system oscillator input to the MCGOUTCLK with the CLKS choose, there has no PLL module, so the system oscillator just can be divided down, can't be doubled.

    But don't worry, if you want to use the 48Mhz core clock, you also can use the internal 48Mhz IRC.

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,417 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Felicita Mercy,

     No, you can't use the external 16Mhz crystal get 48Mhz core clock.

    Please refer to the KL17 reference manual:

pastedImage_1.png

    You can find the system oscillator input to the MCGOUTCLK with the CLKS choose, there has no PLL module, so the system oscillator just can be divided down, can't be doubled.

    But don't worry, if you want to use the 48Mhz core clock, you also can use the internal 48Mhz IRC.

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,416 次查看
felicita
Fresh Out Contributor

Hi Kerry,

Thank you very much for clarifying.

We used internal 48MHz and it is working fine.

Regards,

Felicita Mercy D.

0 项奖励
回复