48 MHz clock generation using external reference in KL17

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

48 MHz clock generation using external reference in KL17

Jump to solution
2,560 Views
felicita
Fresh Out Contributor

Hi all,

We have designed our custom board with MKL17Z256VFM4, with 16 MHz external reference crystal.

Is it possible to generate 48 MHz using external reference clock?

Thank you!

Regards,

Felicita Mercy D.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,443 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Felicita Mercy,

     No, you can't use the external 16Mhz crystal get 48Mhz core clock.

    Please refer to the KL17 reference manual:

pastedImage_1.png

    You can find the system oscillator input to the MCGOUTCLK with the CLKS choose, there has no PLL module, so the system oscillator just can be divided down, can't be doubled.

    But don't worry, if you want to use the 48Mhz core clock, you also can use the internal 48Mhz IRC.

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,444 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Felicita Mercy,

     No, you can't use the external 16Mhz crystal get 48Mhz core clock.

    Please refer to the KL17 reference manual:

pastedImage_1.png

    You can find the system oscillator input to the MCGOUTCLK with the CLKS choose, there has no PLL module, so the system oscillator just can be divided down, can't be doubled.

    But don't worry, if you want to use the 48Mhz core clock, you also can use the internal 48Mhz IRC.

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,443 Views
felicita
Fresh Out Contributor

Hi Kerry,

Thank you very much for clarifying.

We used internal 48MHz and it is working fine.

Regards,

Felicita Mercy D.

0 Kudos
Reply