unable to set breakpoints after update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unable to set breakpoints after update

ソリューションへジャンプ
1,545件の閲覧回数
davepfaltzgraff
Senior Contributor I

It seems that since I have installed the latest updates (a couple days ago), I have not been able to set breakpoints in the Windows GUI. When I click on the bar as normal to set a breakpoint, I get this icon. 48678_48678.pngpastedImage_0.png

 

I am able to right click on the line a perform a "Run to this line." But that's about it.

 

Any hints as to what I'm doing wrong?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,412件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi David,

I think you have 'Skip all breakpoints' enbled:

pastedImage_0.png

See Skipping Breakpoints | MCU on Eclipse

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,413件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi David,

I think you have 'Skip all breakpoints' enbled:

pastedImage_0.png

See Skipping Breakpoints | MCU on Eclipse

Erich

0 件の賞賛
返信
1,412件の閲覧回数
davepfaltzgraff
Senior Contributor I

Right on!

I wasn't even aware of such an option. I've always just deleted all breakpoints when I needed that. (Then reset them again!)

Thanks

0 件の賞賛
返信
1,412件の閲覧回数
rolffreitag
Contributor III

I had the same problem and all IDEs i have worked with before did not had such an option.

0 件の賞賛
返信