make: *** [Project_Settings/Startup_Code/__arm_end.o] Error 1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

make: *** [Project_Settings/Startup_Code/__arm_end.o] Error 1

1,580 次查看
niranjanbc
Contributor IV

I was importing the project from codewarrior to KDS, when I do a build i am getting below error

make: *** [Project_Settings/Startup_Code/__arm_end.o] Error 1

标签 (1)
0 项奖励
回复
2 回复数

1,378 次查看
kirantujare
Contributor IV

Hi Niranjan,
Did you solve the error?
If so, could you help me solve it?

0 项奖励
回复

1,378 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello niranjanbc,

About porting project from CodeWarrior to KDS, there are some attention,

please refer to here :

Importing MCU V10.6 projects (sample, using PE and MQX) under KDS

If still have any question , please contact us !

Hope it helps !

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复